CSL_Aif2Param Struct Reference
[AIF2 Data Structures]

Module specific parameters. More...

#include <csl_aif2.h>


Data Fields

CSL_BitMask8 flags
CSL_Aif2GlobalSetup gSetup


Detailed Description

Module specific parameters.


Field Documentation

CSL_BitMask8 CSL_Aif2Param::flags

Bit mask to be used for selecting link specific parameters. For this module, this is not used as there is only one module specific parameter. So user need not worry about this.

CSL_Aif2GlobalSetup CSL_Aif2Param::gSetup

Global setup structure


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated