CSL_Aif2PdChConfig1 Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2PdCommonSetup. This structure is used for configuring Pd 128 Dma channel configuration 1 register. More...

#include <csl_aif2.h>


Data Fields

Bool bTsWatchDogEn
CSL_Aif2GSMDataFormat DataFormat
Uint8 FrameCounter
Uint8 DioOffset
Uint16 TddEnable


Detailed Description

This is a sub-structure in CSL_Aif2PdCommonSetup. This structure is used for configuring Pd 128 Dma channel configuration 1 register.


Field Documentation

Bool CSL_Aif2PdChConfig1::bTsWatchDogEn

TS: enable OBSAI time stamp watch dog timer (only known use is GSM BB hopping). (Set to 0 for CPRI)

CSL_Aif2GSMDataFormat CSL_Aif2PdChConfig1::DataFormat

GSM data format (Other or GSM UL)

Uint8 CSL_Aif2PdChConfig1::FrameCounter

OBSAI framing counter: Which of 6 framing counter terminal counts should be used for each dma channel. (codes 3'b110 & 3'b111 are reserved)

Uint8 CSL_Aif2PdChConfig1::DioOffset

Offset for DIO DMA mode. Used to align DMA for AxC with different AxC offsets.

Uint16 CSL_Aif2PdChConfig1::TddEnable

PD TDD, disables DMA of whole symbols (CPPI packets), Program as 0xffff for most applications Bit mapped, bit0 --> sym0 of framing FSM (Symbol count above 15 are always enabled)


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated