CSL_Aif2PdChannelConfig Struct Reference
[AIF2 Data Structures]

This structure is used for dynamic configuring the channel parameters of protocol decoder. More...

#include <csl_aif2.h>


Data Fields

Uint8 ChannelNum
CSL_Aif2PdRoute PdRoute
CSL_Aif2PdChConfig PdChConfig
CSL_Aif2PdChConfig1 PdChConfig1
Uint32 TddEnable1
Uint32 TddEnable2
Uint32 TddEnable3
Uint32 TddEnable4
Uint16 PdFrameMsgTc


Detailed Description

This structure is used for dynamic configuring the channel parameters of protocol decoder.


Field Documentation

Uint8 CSL_Aif2PdChannelConfig::ChannelNum

dedicated channel number for this setup

CSL_Aif2PdRoute CSL_Aif2PdChannelConfig::PdRoute

Pd route

CSL_Aif2PdChConfig CSL_Aif2PdChannelConfig::PdChConfig

Pd 128 Dma channel configuration

CSL_Aif2PdChConfig1 CSL_Aif2PdChannelConfig::PdChConfig1

Pd 128 Dma channel configuration 1

Uint32 CSL_Aif2PdChannelConfig::TddEnable1

TDD symbol enable/disable from symbol 16 ~ 47

Uint32 CSL_Aif2PdChannelConfig::TddEnable2

TDD symbol enable/disable from symbol 48 ~ 79

Uint32 CSL_Aif2PdChannelConfig::TddEnable3

TDD symbol enable/disable from symbol 80 ~ 111

Uint32 CSL_Aif2PdChannelConfig::TddEnable4

TDD symbol enable/disable from symbol 112 ~ 143

Uint16 CSL_Aif2PdChannelConfig::PdFrameMsgTc

pd frame message terminal count


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated