CSL_Aif2PdCpriIdLut Struct Reference
[AIF2 Data Structures]

This structure is used for dynamic configuring the cpri Id LUT parameters of protocol decoder. More...

#include <csl_aif2.h>


Data Fields

Uint8 ChannelNum
Uint8 CpriDmaCh
Bool bEnableCpriX
Bool bEnableCpriPkt
Uint8 Cpri8WordOffset


Detailed Description

This structure is used for dynamic configuring the cpri Id LUT parameters of protocol decoder.


Field Documentation

Uint8 CSL_Aif2PdCpriIdLut::ChannelNum

dedicated channel number for this setup

Uint8 CSL_Aif2PdCpriIdLut::CpriDmaCh

DBMF CPRI Stream LUT: AxC:used to map DBM X count to DMA channel. PKT:2 lsb indicates 0-3 PKT packing circuit (assumed 4B/5B encoding)

Bool CSL_Aif2PdCpriIdLut::bEnableCpriX

DBMF CPRI Stream LUT: enable-disable of channel, for each value of DBM X count.

Bool CSL_Aif2PdCpriIdLut::bEnableCpriPkt

DBMF CPRI Stream LUT: dicates the cpri payload is to be used as AxC (normal) or Packet traffic

Uint8 CSL_Aif2PdCpriIdLut::Cpri8WordOffset

Fine AxC offset. Used in the front end of PD to align word data into QWords. bit [1:0] are offset into a QWord. bit[2] give RSA double QWork alignment. Bit[2] and corresponding axc_offset[0] should always be programmed to be identical


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated