CSL_Aif2PdRoute Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2PdCommonSetup. This structure is used for configuring the routing parameters of protocol decoder. More...

#include <csl_aif2.h>


Data Fields

Uint8 RouteTs
Uint8 RouteType
Uint16 RouteAddr
Uint8 RouteLink
CSL_Aif2RouteMask RouteMask


Detailed Description

This is a sub-structure in CSL_Aif2PdCommonSetup. This structure is used for configuring the routing parameters of protocol decoder.


Field Documentation

Uint8 CSL_Aif2PdRoute::RouteTs

OBSAI time stamp in header. Used to extend addressing by using the TS field The number of bits of TS to compare is controlled via the ctrl field.

Uint8 CSL_Aif2PdRoute::RouteType

OBSAI type field in header

Uint16 CSL_Aif2PdRoute::RouteAddr

OBSAI address field in header

Uint8 CSL_Aif2PdRoute::RouteLink

Link number for which to apply this routing rule

CSL_Aif2RouteMask CSL_Aif2PdRoute::RouteMask

controls how many OBSAI time stamp bits to use in the reception routing.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated