CSL_Aif2PdTypeLut Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2PdLinkSetup. This structure is used for configuring the parameters of 32 Pd type LUT. More...

#include <csl_aif2.h>


Data Fields

CSL_Aif2TstampFormat ObsaiTsFormat
CSL_Aif2CrcLen PdCrcType
Bool bEnableCrc
CSL_Aif2PdDataMode PdObsaiMode
Bool bEnableEnetStrip
Bool bEnableCrcHeader


Detailed Description

This is a sub-structure in CSL_Aif2PdLinkSetup. This structure is used for configuring the parameters of 32 Pd type LUT.


Field Documentation

CSL_Aif2TstampFormat CSL_Aif2PdTypeLut::ObsaiTsFormat

PD OBSAI time stamp format selection

CSL_Aif2CrcLen CSL_Aif2PdTypeLut::PdCrcType

PD CRC type selection

Bool CSL_Aif2PdTypeLut::bEnableCrc

enable CRC for this link

CSL_Aif2PdDataMode CSL_Aif2PdTypeLut::PdObsaiMode

OBSAI mode selection between packet and AxC

Bool CSL_Aif2PdTypeLut::bEnableEnetStrip

enable Ethernet strip for this link

Bool CSL_Aif2PdTypeLut::bEnableCrcHeader

enable CRC calculation for OBSAI header


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated