CSL_Aif2PeInFifoControl Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2PeCommonSetup. This structure is used for PE input fifo control register. More...

#include <csl_aif2.h>


Data Fields

Uint8 MFifoWmark
Uint8 MFifoFullLevel
Uint8 SyncSymbol


Detailed Description

This is a sub-structure in CSL_Aif2PeCommonSetup. This structure is used for PE input fifo control register.


Field Documentation

Uint8 CSL_Aif2PeInFifoControl::MFifoWmark

Set water mark per channel. Water mark controls fill level for which lower/higher fetch rate is issued

Uint8 CSL_Aif2PeInFifoControl::MFifoFullLevel

Set full level per channel. Full level controls halt of data fetch to prevent overflow

Uint8 CSL_Aif2PeInFifoControl::SyncSymbol

Normally set to 0. First non-tdd symbol of frame. Used for startup sync with DMA


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated