CSL_Aif2PeModuloRule Struct Reference
[AIF2 Data Structures]

This structure is used for dynamic configuring the Modulo rule parameters of protocol encoder. More...

#include <csl_aif2.h>


Data Fields

Uint16 RuleNum
CSL_Aif2ModuloTc PeModuloTc


Detailed Description

This structure is used for dynamic configuring the Modulo rule parameters of protocol encoder.


Field Documentation

Uint16 CSL_Aif2PeModuloRule::RuleNum

dedicated rule number for this setup

CSL_Aif2ModuloTc CSL_Aif2PeModuloRule::PeModuloTc

Modulo terminal count structure


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated