CSL_Aif2PeObsaiHeader Struct Reference
[AIF2 Data Structures]

This structure is used for dynamic configuring the obsai header parameters of protocol encoder. More...

#include <csl_aif2.h>


Data Fields

Uint8 ChannelNum
Uint8 PeChObsaiType
Uint8 PeChObsaiTs
Uint16 PeChObsaiAddr
CSL_Aif2ObsaiTsMask PeChObsaiTsMask
CSL_Aif2TstampFormat PeChObsaiTsfomat


Detailed Description

This structure is used for dynamic configuring the obsai header parameters of protocol encoder.


Field Documentation

Uint8 CSL_Aif2PeObsaiHeader::ChannelNum

dedicated channel number for this setup

Uint8 CSL_Aif2PeObsaiHeader::PeChObsaiType

PE DMA channel OBSAI time stamp value which is inserted into the frame

Uint8 CSL_Aif2PeObsaiHeader::PeChObsaiTs

PE DMA channel OBSAI type value which is inserted into the frame

Uint16 CSL_Aif2PeObsaiHeader::PeChObsaiAddr

PE DMA channel OBSAI address value which is inserted into the frame

CSL_Aif2ObsaiTsMask CSL_Aif2PeObsaiHeader::PeChObsaiTsMask

PE DMA channel OBSAI time stamp mask value which is inserted into the frame

CSL_Aif2TstampFormat CSL_Aif2PeObsaiHeader::PeChObsaiTsfomat

PE DMA channel OBSAI time stamp generation algorithm


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated