CSL_Aif2RmStatus0 Struct Reference
[AIF2 Data Structures]

This object contains the aif2 Rm link status0 information. More...

#include <csl_aif2.h>


Data Fields

CSL_Aif2RmSyncState rmSyncStatus
Bool rmLos
Bool rmNumLosDetect
Bool rmLoc
Bool rmFifoOverflow


Detailed Description

This object contains the aif2 Rm link status0 information.


Field Documentation

CSL_Aif2RmSyncState CSL_Aif2RmStatus0::rmSyncStatus

Indicates that status of the Frame Sync state machine

Bool CSL_Aif2RmStatus0::rmLos

Active when RX state machine is in ST0, inactive otherwise

Bool CSL_Aif2RmStatus0::rmNumLosDetect

Detects when num_los counter has reached the programable los_det_thold limit

Bool CSL_Aif2RmStatus0::rmLoc

The clock watchdog circuit detected a missing clock

Bool CSL_Aif2RmStatus0::rmFifoOverflow

Active after an RM FIFO overflow


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated