CSL_Aif2RmStatus1 Struct Reference
[AIF2 Data Structures]

This object contains the aif2 Rm link status1 information. More...

#include <csl_aif2.h>


Data Fields

Uint16 rmNumLos
Uint16 rmLcvCountValue


Detailed Description

This object contains the aif2 Rm link status1 information.


Field Documentation

Uint16 CSL_Aif2RmStatus1::rmNumLos

Represents the number of los detect

Uint16 CSL_Aif2RmStatus1::rmLcvCountValue

Number of Line Code Violations counted since last cleared and enabled. Range 0 to 65,535


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated