CSL_Aif2RmStatus2 Struct Reference
[AIF2 Data Structures]

This object contains the aif2 Rm link status2 information. More...

#include <csl_aif2.h>


Data Fields

Uint16 rmClockQuality
Uint8 rmScrValue


Detailed Description

This object contains the aif2 Rm link status2 information.


Field Documentation

Uint16 CSL_Aif2RmStatus2::rmClockQuality

A value that represents the quality, relative frequency, of the received Serdes clock. Range 0 to 65,535

Uint8 CSL_Aif2RmStatus2::rmScrValue

Indicates the captured scrambling code, only when configuration bit scr_en = 1.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated