CSL_Aif2RmStatus4 Struct Reference
[AIF2 Data Structures]

This object contains the aif2 Rm link status4 information. More...

#include <csl_aif2.h>


Data Fields

Uint8 rmL1Version
Uint8 rmL1Startup
Bool rmL1RST
Bool rmL1RAI
Bool rmL1SDI
Bool rmL1LOS
Bool rmL1LOF
Bool rmL1PointerP


Detailed Description

This object contains the aif2 Rm link status4 information.


Field Documentation

Uint8 CSL_Aif2RmStatus4::rmL1Version

Received protocol version, Z.2.0

Uint8 CSL_Aif2RmStatus4::rmL1Startup

Received start up information, Z.66.0

Bool CSL_Aif2RmStatus4::rmL1RST

Received reset, Z.130.0, b0

Bool CSL_Aif2RmStatus4::rmL1RAI

Received rai, Z.130.0, b1

Bool CSL_Aif2RmStatus4::rmL1SDI

Received sdi, Z.130.0, b2

Bool CSL_Aif2RmStatus4::rmL1LOS

Received los, Z.130.0, b3

Bool CSL_Aif2RmStatus4::rmL1LOF

Received lof, Z.130.0, b4

Bool CSL_Aif2RmStatus4::rmL1PointerP

Received Pointer P


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated