![]() |
![]() |
#include <csl_aif2.h>
Data Fields | |
| CSL_Aif2LinkIndex | CiSelect |
| Bool | bEnableEmptyMsg |
| CSL_Aif2RtConfig | RtConfig |
The CI Select bits indicate the selected inbound link for the retransmitted data path
The Empty Message Enable Bit configures the RT block to insert an empty message in the event that a message is discovered to have a code violation in the header. The configuration is valid in OBSAI mode only.
The RT Configuration field configures the mode of operation of the RT block