CSL_Aif2RtStatus Struct Reference
[AIF2 Data Structures]

This object contains the aif2 Rt link status information. More...

#include <csl_aif2.h>


Data Fields

Bool rtHeaderError
Bool rtEmptyMessage
Bool rtFifoUnderflow
Bool rtFifoOverflow
Bool rtFrameError


Detailed Description

This object contains the aif2 Rt link status information.


Field Documentation

Bool CSL_Aif2RtStatus::rtHeaderError

Indicates a header error has occurred

Bool CSL_Aif2RtStatus::rtEmptyMessage

Indicates an empty message was inserted

Bool CSL_Aif2RtStatus::rtFifoUnderflow

Indicates an Underflow of the FIFO has occurred

Bool CSL_Aif2RtStatus::rtFifoOverflow

Indicates an Overflow of the FIFO has occurred

Bool CSL_Aif2RtStatus::rtFrameError

Indicates a frame error of the FIFO has occurred


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated