![]() |
![]() |
#include <csl_aif2.h>
Data Fields | |
| Uint8 | sdTxBusWidth |
| Bool | sdTxTestFail |
The transmitter bus bandwidth is fixed in hardware to 20 bits and is not configurable through an MMR. However the value that reflects a 20 bit bus width will be read of the configuration register is read
Test Failure. Driven high when an error is encountered during a test sequence executed on an individual channel. Synchronous to TXBCLK