CSL_Aif2TmLinkSetup Struct Reference
[AIF2 Data Structures]

This is a sub-structure in CSL_Aif2LinkSetup. This structure is used for configuring the parameters of the TM. More...

#include <csl_aif2.h>


Data Fields

Bool bEnableTmLink
Bool bEnableRmLos
Uint8 SeedValue
Bool bEnableScrambler
CSL_Aif2CpriTmSetup pCpriTmSetup


Detailed Description

This is a sub-structure in CSL_Aif2LinkSetup. This structure is used for configuring the parameters of the TM.


Field Documentation

Bool CSL_Aif2TmLinkSetup::bEnableTmLink

Boolean indicating if Tm link is to be enabled

Bool CSL_Aif2TmLinkSetup::bEnableRmLos

Boolean indicating if Loss of Sync on Rm is to be enabled

Uint8 CSL_Aif2TmLinkSetup::SeedValue

seed value for Tx scramber initialization

Bool CSL_Aif2TmLinkSetup::bEnableScrambler

Boolean indicating if Tm Scrambler is to be enabled

CSL_Aif2CpriTmSetup CSL_Aif2TmLinkSetup::pCpriTmSetup

pointer to CPRI setup for TM


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated