CSL_CPSW_3GF_ALE_OUIADDR_ENTRY Struct Reference
[CPSW_3GF Data Structures]

Holds the ALE OUI Unicast Address Table entry configuration. More...

#include <csl_cpsw_3gf.h>


Data Fields

Uint8 ouiAddress [3]
CSL_CPSW_3GF_ALE_UCASTTYPE ucastType


Detailed Description

Holds the ALE OUI Unicast Address Table entry configuration.


Field Documentation

Uint8 CSL_CPSW_3GF_ALE_OUIADDR_ENTRY::ouiAddress[3]

OUI Unicast address

CSL_CPSW_3GF_ALE_UCASTTYPE CSL_CPSW_3GF_ALE_OUIADDR_ENTRY::ucastType

Unicast type


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated