CSL_CPSW_3GF_ALE_PORTCONTROL Struct Reference
[CPSW_3GF Data Structures]

Holds the ALE Port control register info. More...

#include <csl_cpsw_3gf.h>


Data Fields

CSL_CPSW_3GF_ALE_PORTSTATE portState
Uint32 dropUntaggedEnable
Uint32 vidIngressCheckEnable
Uint32 noLearnModeEnable
Uint32 mcastLimit
Uint32 bcastLimit


Detailed Description

Holds the ALE Port control register info.


Field Documentation

CSL_CPSW_3GF_ALE_PORTSTATE CSL_CPSW_3GF_ALE_PORTCONTROL::portState

Port state

Uint32 CSL_CPSW_3GF_ALE_PORTCONTROL::dropUntaggedEnable

Drop non-VLAN tagged ingress packets?

Uint32 CSL_CPSW_3GF_ALE_PORTCONTROL::vidIngressCheckEnable

VLAN ID Ingress check enable

Uint32 CSL_CPSW_3GF_ALE_PORTCONTROL::noLearnModeEnable

No learn mode enable

Uint32 CSL_CPSW_3GF_ALE_PORTCONTROL::mcastLimit

Multicast packet rate limit

Uint32 CSL_CPSW_3GF_ALE_PORTCONTROL::bcastLimit

Broadcast packet rate limit


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated