CSL_CPSW_3GF_CONTROL Struct Reference
[CPSW_3GF Data Structures]

Holds CPSW control register contents. More...

#include <csl_cpsw_3gf.h>


Data Fields

Uint32 fifoLb
Uint32 vlanAware
Uint32 p0Enable
Uint32 p0PassPriTag
Uint32 p1PassPriTag
Uint32 p2PassPriTag


Detailed Description

Holds CPSW control register contents.


Field Documentation

Uint32 CSL_CPSW_3GF_CONTROL::fifoLb

FIFO loopback mode

Uint32 CSL_CPSW_3GF_CONTROL::vlanAware

Vlan aware mode

Uint32 CSL_CPSW_3GF_CONTROL::p0Enable

Port 0 Enable

Uint32 CSL_CPSW_3GF_CONTROL::p0PassPriTag

Port 0 Pass Priority Tagged

Uint32 CSL_CPSW_3GF_CONTROL::p1PassPriTag

Port 1 Pass Priority Tagged

Uint32 CSL_CPSW_3GF_CONTROL::p2PassPriTag

Port 2 Pass Priority Tagged


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated