CSL_CPSW_3GF_PORTSTAT Struct Reference
[CPSW_3GF Data Structures]

Holds Port Statistics Enable register contents. More...

#include <csl_cpsw_3gf.h>


Data Fields

Uint32 p0AStatEnable
Uint32 p0BStatEnable
Uint32 p1StatEnable
Uint32 p2StatEnable


Detailed Description

Holds Port Statistics Enable register contents.


Field Documentation

Uint32 CSL_CPSW_3GF_PORTSTAT::p0AStatEnable

Port 0 Statistics A Enable bit

Uint32 CSL_CPSW_3GF_PORTSTAT::p0BStatEnable

Port 0 Statistics B Enable bit

Uint32 CSL_CPSW_3GF_PORTSTAT::p1StatEnable

Port 1 Statistics Enable bit

Uint32 CSL_CPSW_3GF_PORTSTAT::p2StatEnable

Port 2 Statistics Enable bit


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated