CSL_CPTS_EVENTINFO Struct Reference
[CPTS Data Structures]

Holds Time sync event info contents. More...

#include <csl_cpts.h>


Data Fields

Uint32 timeStamp
Uint32 seqId
Uint32 msgType
Uint32 eventType
Uint32 portNo


Detailed Description

Holds Time sync event info contents.


Field Documentation

Uint32 CSL_CPTS_EVENTINFO::timeStamp

Time stamp read from the CPTS EVENT_LOW register

Uint32 CSL_CPTS_EVENTINFO::seqId

Sequence Id read from CPTS EVENT_HIGH register

Uint32 CSL_CPTS_EVENTINFO::msgType

Message Type read from CPTS EVENT_HIGH register

Uint32 CSL_CPTS_EVENTINFO::eventType

Event Type read from CPTS EVENT_HIGH register

Uint32 CSL_CPTS_EVENTINFO::portNo

Port number read from CPTS EVENT_HIGH register


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated