CSL_CPTS_VERSION Struct Reference
[CPTS Data Structures]

Holds the Time sync submodule's version info. More...

#include <csl_cpts.h>


Data Fields

Uint32 minorVer
Uint32 majorVer
Uint32 rtlVer
Uint32 id


Detailed Description

Holds the Time sync submodule's version info.


Field Documentation

Uint32 CSL_CPTS_VERSION::minorVer

Minor version value

Uint32 CSL_CPTS_VERSION::majorVer

Major version value

Uint32 CSL_CPTS_VERSION::rtlVer

RTL version value

Uint32 CSL_CPTS_VERSION::id

Identification value


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated