![]() |
![]() |
#include <csl_edma3.h>
Data Fields | |
| Int | region |
| CSL_BitMask32 | drae |
| CSL_BitMask32 | draeh |
An object of this type is allocated by the user and its address is passed as a parameter to the CSL_edma3GetHwStatus when
this field needs to be initialiazed by the user before issuing the command specifying the region for which attributes need to be set
| CSL_BitMask32 CSL_Edma3CmdDrae::drae |
DRAE Setting for the region
| CSL_BitMask32 CSL_Edma3CmdDrae::draeh |
DRAEH Setting for the region