CSL_Edma3CmdIntr Struct Reference
[EDMA3 Data Structures]

Edma Control/Query Control Command structure for issuing commands for Interrupt related APIs An object of this type is allocated by the user and its address is passed to the Control API. More...

#include <csl_edma3.h>


Data Fields

Int region
CSL_BitMask32 intr
CSL_BitMask32 intrh


Detailed Description

Edma Control/Query Control Command structure for issuing commands for Interrupt related APIs An object of this type is allocated by the user and its address is passed to the Control API.


Field Documentation

Int CSL_Edma3CmdIntr::region

Input field:- this field needs to be initialized by the user before issuing the query/command

CSL_BitMask32 CSL_Edma3CmdIntr::intr

Input/Output field:- this needs to be filled by the user in case of issuing a COMMAND or it will be filled in by the CSL when used with a QUERY

CSL_BitMask32 CSL_Edma3CmdIntr::intrh

Input/Output:- this needs to be filled by the user in case of issuing a COMMAND or it will be filled in by the CSL when used with a QUERY


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated