![]() |
![]() |
#include <csl_edma3.h>
Data Fields | |
| Int | region |
| CSL_BitMask32 | qrae |
An object of this type is allocated by the user and its address is passed as a parameter to the CSL_edma3GetHwStatus/CSL_edma3HwControl with the relevant command.
this field needs to be initialized by the user before issuing the query/command
| CSL_BitMask32 CSL_Edma3CmdQrae::qrae |
this needs to be filled by the user in case of issuing a COMMAND or it will be filled in by the CSL when used with a QUERY