CSL_Edma3CtrlErrStat Struct Reference
[EDMA3 Data Structures]

Edma Controller Error Status. More...

#include <csl_edma3.h>


Data Fields

CSL_BitMask16 error
Bool exceedTcc


Detailed Description

Edma Controller Error Status.

An object of this type is allocated by the user and its address is passed as a parameter to the CSL_edma3GetControllerError() /CSL_edma3GetHwStatus().


Field Documentation

CSL_BitMask16 CSL_Edma3CtrlErrStat::error

Bit Mask of the Que Threshold Errors

Bool CSL_Edma3CtrlErrStat::exceedTcc

Whether number of permissible outstanding Tcc's is exceeded


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated