CSL_Edma3HwDmaChannelSetup Struct Reference
[EDMA3 Data Structures]

QDMA Edma Channel Setup. More...

#include <csl_edma3.h>


Data Fields

CSL_Edma3Que que
Uint16 paramNum


Detailed Description

QDMA Edma Channel Setup.

An array of such objects are allocated by the user and address initialized in the CSL_Edma3HwSetup structure which is passed CSL_edma3HwSetup()


Field Documentation

CSL_Edma3Que CSL_Edma3HwDmaChannelSetup::que

Que number for the channel

Uint16 CSL_Edma3HwDmaChannelSetup::paramNum

Parameter set mapping for the channel.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated