![]() |
![]() |
#include <csl_edma3.h>
Data Fields | |
| CSL_Edma3Que | que |
| Uint16 | paramNum |
| Uint8 | triggerWord |
An array of such objects are allocated by the user and address initialized in the CSL_Edma3HwSetup structure which is passed CSL_edma3HwSetup()
Que number for the channel
Parameter set mapping for the channel.
Trigger word for the QDMA channels.