![]() |
![]() |
#include <csl_edma3.h>
Data Fields | |
| Uint32 | addr |
| CSL_BitMask16 | error |
| Uint16 | fid |
An object of this type is allocated by the user and its address is passed as a parameter to the CSL_edma3GetMemoryFaultError() / CSL_edma3GetHwStatus() with the relevant command. This is relevant only is MPEXIST is present for a given device.
| Uint32 CSL_Edma3MemFaultStat::addr |
Memory Protection Fault Address
| CSL_BitMask16 CSL_Edma3MemFaultStat::error |
Bit Mask of the Errors
| Uint16 CSL_Edma3MemFaultStat::fid |
Faulted ID