![]() |
![]() |
#include <csl_edma3.h>
Data Fields | |
| Uint32 | revision |
| Uint32 | config |
An object of this type is allocated by the user and its address is passed as a parameter to the CSL_edma3GetInfo() /CSL_edma3GetHwStatus().
| Uint32 CSL_Edma3QueryInfo::revision |
Revision/Periperhal id of the EDMA3 Channel Controller
| Uint32 CSL_Edma3QueryInfo::config |
Channel Controller Configuration obtained from the CCCFG register