![]() |
![]() |
#include <csl_idma.h>
Data Fields | |
| Uint32 | isPending:1 |
| Boolean Flag that indicates if any pending transfers exist on the iDMA channel 1/channel 0. | |
| Uint32 | isActive:1 |
| Boolean Flag that indicates if any active transfers exist on the iDMA channel 1/channel 0. | |
| Uint32 CSL_IDMA_STATUS::isPending |
Boolean Flag that indicates if any pending transfers exist on the iDMA channel 1/channel 0.
Set when control registers are written to by the CPU and there is already an active transfer in progress (ACTV=1) and cleared when the pending transfer becomes active.
| Uint32 CSL_IDMA_STATUS::isActive |
Boolean Flag that indicates if any active transfers exist on the iDMA channel 1/channel 0.
Set when channel 0/1 begins reading data from the source address and cleared following the write to the destination address.