CSL_IntcEventHandlerRecord Struct Reference
[INTC Data Structures]

#include <csl_intc.h>


Data Fields

CSL_IntcEventHandler handler
void * arg


Detailed Description

Event Handler Record

Used to set-up the event-handler using CSL_intcPlugEventHandler(..)


Field Documentation

CSL_IntcEventHandler CSL_IntcEventHandlerRecord::handler

pointer to the event handler

void* CSL_IntcEventHandlerRecord::arg

the argument to be passed to the handler when it is invoked


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated