CSL_MDIO_USERACCESS Struct Reference
[MDIO Data Structures]

Holds the MDIO User Access Register contents. More...

#include <csl_mdio.h>


Data Fields

Uint16 data
Uint32 phyAddr
Uint32 regAddr
Uint32 ack
Uint32 go


Detailed Description

Holds the MDIO User Access Register contents.


Field Documentation

Uint16 CSL_MDIO_USERACCESS::data

Data bits

Uint32 CSL_MDIO_USERACCESS::phyAddr

Phy Device Address

Uint32 CSL_MDIO_USERACCESS::regAddr

Register Address

Uint32 CSL_MDIO_USERACCESS::ack

Acknowledgment bit

Uint32 CSL_MDIO_USERACCESS::go

GO bit


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated