CSL_MDIO_VERSION Struct Reference
[MDIO Data Structures]

Holds the MDIO peripheral's version info. More...

#include <csl_mdio.h>


Data Fields

Uint32 revMin
Uint32 revMaj
Uint32 modId


Detailed Description

Holds the MDIO peripheral's version info.


Field Documentation

Uint32 CSL_MDIO_VERSION::revMin

Minor revision value

Uint32 CSL_MDIO_VERSION::revMaj

Major revision value

Uint32 CSL_MDIO_VERSION::modId

Identifies the type of peripheral


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated