CSL_SGMII_STATUS Struct Reference
[SGMII Data Structures]

Holds the SGMII status info. More...

#include <csl_cpsgmii.h>


Data Fields

Uint32 bIsLinkUp
Uint32 bIsAutoNegError
Uint32 bIsAutoNegComplete
Uint32 bIsLocked


Detailed Description

Holds the SGMII status info.


Field Documentation

Uint32 CSL_SGMII_STATUS::bIsLinkUp

Link Status

Uint32 CSL_SGMII_STATUS::bIsAutoNegError

Auto-negotiation error indicator

Uint32 CSL_SGMII_STATUS::bIsAutoNegComplete

Auto-negotiation completion status

Uint32 CSL_SGMII_STATUS::bIsLocked

Lock Status


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated