CSL_TAC_BETI_status Struct Reference
[TAC Back-End Data Structures]

The descriptor specifies the parameters obtained from the BETI status register. More...

#include <csl_tac_regsBEAux.h>


Data Fields

CSL_TAC_BETI_statusBit sgcp0Status
CSL_TAC_BETI_statusBit sgcp1Status


Detailed Description

The descriptor specifies the parameters obtained from the BETI status register.


Field Documentation

CSL_TAC_BETI_statusBit CSL_TAC_BETI_status::sgcp0Status

Status of the SGCP 0

CSL_TAC_BETI_statusBit CSL_TAC_BETI_status::sgcp1Status

Status of the SGCP 1


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated