CSL_TAC_FE_PeripheralId_req Struct Reference
[TAC Front-End Data Structures]

This descriptor specifies the fields of the peripheral Id register. More...

#include <csl_tac_regsFEAux.h>


Data Fields

Uint8 minorRevNum
Uint8 customRevNum
Uint8 majorRevNum
Uint8 rtlRevNum
Uint16 peripheralId
Uint8 scheme


Detailed Description

This descriptor specifies the fields of the peripheral Id register.


Field Documentation

Uint8 CSL_TAC_FE_PeripheralId_req::minorRevNum

Specifies the Minor Revision number.

Uint8 CSL_TAC_FE_PeripheralId_req::customRevNum

Specifies the Custom Revision number.

Uint8 CSL_TAC_FE_PeripheralId_req::majorRevNum

Specifies the Major Revision number.

Uint8 CSL_TAC_FE_PeripheralId_req::rtlRevNum

Specifies the RTL Revision number.

Uint16 CSL_TAC_FE_PeripheralId_req::peripheralId

Specifies the Peripheral Id (0x807)

Uint8 CSL_TAC_FE_PeripheralId_req::scheme

Specifies the Scheme (0x1 - New Scheme).


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated