CSL_TAC_SGCP_cycleOverflowStatus Struct Reference
[TAC SGCP Data Structures]

This descriptor specifies the parameters obtained when reading the cycle overflow status register. More...

#include <csl_tac_regsSGCPAux.h>


Data Fields

Uint16 iteNb
Uint8 overflowFlag
Uint8 pageIdx
Uint8 taskIdx


Detailed Description

This descriptor specifies the parameters obtained when reading the cycle overflow status register.


Field Documentation

Uint16 CSL_TAC_SGCP_cycleOverflowStatus::iteNb

Denotes the iteration number.

Uint8 CSL_TAC_SGCP_cycleOverflowStatus::overflowFlag

Denotes the overflow status.

Uint8 CSL_TAC_SGCP_cycleOverflowStatus::pageIdx

Denotes the page index.

Uint8 CSL_TAC_SGCP_cycleOverflowStatus::taskIdx

Denotes the task index.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated