CSL_TAC_SGCP_symbolBuffMissStatus Struct Reference
[TAC SGCP Data Structures]

This descriptor specifies the parameters obtained when reading the symbol buffer miss status register. More...

#include <csl_tac_regsSGCPAux.h>


Data Fields

Uint16 iteNb
Uint8 writeMissFlag
Uint8 pageIdx
Uint8 taskIdx


Detailed Description

This descriptor specifies the parameters obtained when reading the symbol buffer miss status register.


Field Documentation

Uint16 CSL_TAC_SGCP_symbolBuffMissStatus::iteNb

Denotes the iteration number.

Uint8 CSL_TAC_SGCP_symbolBuffMissStatus::writeMissFlag

Denotes the cycle overflow flag

Uint8 CSL_TAC_SGCP_symbolBuffMissStatus::pageIdx

Denotes the page index.

Uint8 CSL_TAC_SGCP_symbolBuffMissStatus::taskIdx

Denotes the task index.


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated