CSL_TmrBaseAddress Struct Reference
[TIMER Data Structures]

This structure contains the base-address information for the peripheral instance. More...

#include <csl_tmr.h>


Data Fields

CSL_TmrRegsOvly regs


Detailed Description

This structure contains the base-address information for the peripheral instance.


Field Documentation

CSL_TmrRegsOvly CSL_TmrBaseAddress::regs

Base-address of the configuration registers of the peripheral


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated