CSL_TmrConfig Struct Reference
[TIMER Data Structures]

Config-structure Used to configure the GP timer using CSL_tmrHwSetupRaw(). More...

#include <csl_tmr.h>


Data Fields

Uint32 CNTLO
Uint32 CNTHI
Uint32 PRDLO
Uint32 PRDHI
Uint32 TCR
Uint32 TGCR
Uint32 WDTCR


Detailed Description

Config-structure Used to configure the GP timer using CSL_tmrHwSetupRaw().


Field Documentation

Uint32 CSL_TmrConfig::CNTLO

Timer Counter Register Low

Uint32 CSL_TmrConfig::CNTHI

Timer Counter Register High

Uint32 CSL_TmrConfig::PRDLO

Timer Period Register Low

Uint32 CSL_TmrConfig::PRDHI

Timer Period Register High

Uint32 CSL_TmrConfig::TCR

Timer Control Register

Uint32 CSL_TmrConfig::TGCR

Timer Global Control Register

Uint32 CSL_TmrConfig::WDTCR

Watchdog Timer Control Register


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated