![]() |
![]() |
#include <csl_xmc.h>
Data Fields | |
| Uint32 | local |
| Uint32 | sr |
| Uint32 | sw |
| Uint32 | sx |
| Uint32 | ur |
| Uint32 | uw |
| Uint32 | ux |
| Uint32 CSL_XMC_MPFSR::local |
Local Access ?
| Uint32 CSL_XMC_MPFSR::sr |
When set, indicates a Supervisor Read Request
| Uint32 CSL_XMC_MPFSR::sw |
When set, indicates a Supervisor Write Request
| Uint32 CSL_XMC_MPFSR::sx |
When set, indicates a Supervisor program fetch Request
| Uint32 CSL_XMC_MPFSR::ur |
When set, indicates a User Read Request
| Uint32 CSL_XMC_MPFSR::uw |
When set, indicates a User Write Request
| Uint32 CSL_XMC_MPFSR::ux |
When set, indicates a User program fetch Request