CSL_XMC_XMPAXL Struct Reference
[XMC Data Structures]

This is the definition of CSL_XMC_XMPAXL. More...

#include <csl_xmc.h>


Data Fields

Uint32 rAddr
Uint32 sr
Uint32 sw
Uint32 sx
Uint32 ur
Uint32 uw
Uint32 ux


Detailed Description

This is the definition of CSL_XMC_XMPAXL.


Field Documentation

Uint32 CSL_XMC_XMPAXL::rAddr

Replacement Address

Uint32 CSL_XMC_XMPAXL::sr

When set, supervisor may read from segment

Uint32 CSL_XMC_XMPAXL::sw

When set, supervisor may write to segment

Uint32 CSL_XMC_XMPAXL::sx

When set, supervisor may execute from segment

Uint32 CSL_XMC_XMPAXL::ur

When set, user may read from segment

Uint32 CSL_XMC_XMPAXL::uw

When set, user may write to segment

Uint32 CSL_XMC_XMPAXL::ux

When set, user may execute from segment


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated