SRIO Error Rate.
More...
#include <csl_srio.h>
Detailed Description
SRIO Error Rate.
This structure is used to store the error rate CSR configuration which is used to monitor and control the port physical layer errors.
The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated