SRIO Type 9 Message Description.
More...
#include <csl_srio.h>
Detailed Description
SRIO Type 9 Message Description.
This structure is used to define the TYPE9 Message. This is then used to MAP Type9 messages to a specific destination queue.
The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated