![]() |
![]() |
#include <csl_vcp2.h>
Data Fields | |
| Uint32 | ic0 |
| Uint32 | ic1 |
| Uint32 | ic2 |
| Uint32 | ic3 |
| Uint32 | ic4 |
| Uint32 | ic5 |
| Uint32 VCP2_ConfigIc::ic0 |
Value of VCP input configuration register 0
| Uint32 VCP2_ConfigIc::ic1 |
Value of VCP input configuration register 1
| Uint32 VCP2_ConfigIc::ic2 |
Value of VCP input configuration register 2
| Uint32 VCP2_ConfigIc::ic3 |
Value of VCP input configuration register 3
| Uint32 VCP2_ConfigIc::ic4 |
Value of VCP input configuration register 4
| Uint32 VCP2_ConfigIc::ic5 |
Value of VCP input configuration register 5