VCP2_Errors Struct Reference
[VCP2 Data Structures]

#include <csl_vcp2.h>


Data Fields

Bool tbnaErr
Bool ftlErr
Bool fctlErr
Bool maxminErr
Bool symxErr
Bool symrErr


Detailed Description

VCP Error structure


Field Documentation

Bool VCP2_Errors::tbnaErr

Traceback mode error

Bool VCP2_Errors::ftlErr

Frame length error

Bool VCP2_Errors::fctlErr

Reliability + convergence distance error

Bool VCP2_Errors::maxminErr

Max-Min error

Bool VCP2_Errors::symxErr

SYMX error

Bool VCP2_Errors::symrErr

SYMR error


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated