VCP2_Poly Struct Reference
[VCP2 Data Structures]

#include <csl_vcp2.h>


Data Fields

Uint8 poly0
Uint8 poly1
Uint8 poly2
Uint8 poly3


Detailed Description

VCP generator polynomials structure


Field Documentation

Uint8 VCP2_Poly::poly0

Generator polynomial 0

Uint8 VCP2_Poly::poly1

Generator polynomial 1

Uint8 VCP2_Poly::poly2

Generator polynomial 2

Uint8 VCP2_Poly::poly3

Generator polynomial 3


The documentation for this struct was generated from the following file:
Copyright 2011, Texas Instruments Incorporated