This project is made by TI and it is used to test Nyquist Hyperlink(vUSR) module on EVM. this example support local internal loopback mode and two DSP mode together. 

Here is the test procedure that the user could follow.
1. compile the project with Debug mode and get Hyperlink_EVM_example_LE.out file  
2. turn on the EVM and connect the device by using daisy chain mode ccxml file
3. load .out file for both DSP0 core0 and DSP1 core0
4. run two DSPs at the same time and check console window to check the result

This project was tested with CPPI and QMSS LLD and CSL from PDK 10011 version.
this project used two vUSR data segment (one for remote QM and the other for remote memory region in MSMC)